STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 912600 baud rate criteria on UART1 interface?

Hi!I am operating on an STM32F446 chip and I have the following issue:I tested out a communication system where I attached a 912600 baud communication with another device via UART1 on a STM32f446 NUCLEO Board. All worked out well, no errors or other ...

NGros by Associate III
  • 4416 Views
  • 5 replies
  • 0 kudos

FDCAN Message RAM fixed organization

Hi, I've developed a CAN driver for STM32H7 and greatly appreciated the capability to modulate FIFO buffers elements number and size. I am now porting such a driver to STM32L5 but It looks like this is not possible in the STM32L5, where the FIFOs hav...

Resolved! GPIO to ADC channel mapping in STM32F105RBT.

Hello,I'm currently working on an application using STM32F105 uC.I want to use some GPIO as analog input, so I need to use the ADC converter.It seems that each channel is linked to one ADC channel. I have found some table with this mapping for other ...

0693W00000FA0r0QAD.png
DSimo.1 by Associate
  • 3364 Views
  • 2 replies
  • 0 kudos

Resolved! Error in CAN transmission normal mode

I am using 2 microcontrollers STM32F103ZETx as transmitter and STM32F730R8 as reciever. So my CAN is coming into initialization mode but has some issues in CAN normal mode. SLAK=0 , INAK=1(should be 0) and INRQ = 1(should be 0) for can normal mode.1....

SMitt.2 by Associate II
  • 2848 Views
  • 3 replies
  • 0 kudos

VCP with STM32F429I DISCO

I don't understand why i can't use VCP on my STM32F429I-DISCO even if UART RX /TX pin are connected to the USB-ST-link. I know I have to flash this ST-link V2 to V2.1 to have the VCP activated but i can't do that.You can see on the attached schematic...

0693W00000FACvJQAX.png
doddonny by Associate II
  • 1675 Views
  • 2 replies
  • 0 kudos

STM32 I2C Slave mode HAL bug

Recently I have tried to implement a solution employing I2C interface in slave mode.The solution follows the pattern presented in the official I2C_TwoBoards_RestartAdvComIT example available in CubeMX packages and another solution presented here: STM...

TDJ by Lead
  • 2670 Views
  • 2 replies
  • 1 kudos

FMC/FSMC ECC computation

Hello, guys!I have a quick question about FSMC's ECC routine.From what I understood, the workflow goes like this:1) Enable ECC computationSET_BIT(hnand->Instance->PCR, FMC_PCR_ECCEN);2) Write data to the target device3) Get the computed ECCwhile (__F...

PMera.1 by Associate III
  • 1762 Views
  • 2 replies
  • 0 kudos