STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743ZI UART Tx with DMA doesn't want to turn on

Hi guys, its been a while and I hope everyone is well and safe.Using a STM32H743ZIReference Manuel I am having issues turning on the DMA1 stream associated to the UART4 Tx, in this case DMA1_Stream1. The DMA is setup as a One Shot mode (Normal Mode) ...

CLeo.1 by Senior II
  • 2091 Views
  • 5 replies
  • 0 kudos

STM32f746G_DISCO board sdram configuration quesiton

Hi, In the STM32F746G_DISCO board, FMC_SDRAM example, how to decide these parameters? Which section does it specify from sdram MT48LC4M32B2B5 datasheet? SDRAM_Timing.LoadToActiveDelay   = 2; SDRAM_Timing.ExitSelfRefreshDelay = 6; SDRAM_Timing.SelfRe...

JChen.24 by Associate III
  • 1057 Views
  • 1 replies
  • 0 kudos

How to set up the adc sampling time.

Hi,I am using ADC of STM32H743ZI which is configured as 16 bit, ADC clock =36.5MHz,Tsampling=1.5cycles in continuous conversion mode . I am using DMA technique to collect the data using a buffer size of 4096 in circular mode.The input is sine wave o...

GHARI.1 by Associate II
  • 20220 Views
  • 18 replies
  • 0 kudos

UART information is shifted by 1 byte when I connect my STM32G474RE directly to my PC and use a terminal program to send information to control things. It fixes itself after resetting the board.

For example, if I send 1000, it will be received as 0100 on the STM board. I send what I received in the Rxcallback function. My program doesn't work, so I know this is the case. This issue stops after I hit the RESET switch on my board. Now, my iss...

Resolved! Availability of FDCAN peripheral on port C pins of STM32G0B1RE

Hi,Parsing the datasheet DS13560 of the STM32G0B1RE device, there is a discrepency between table 12, where some pins of port C have the FDCAN peripheral listed as alternate function, however it is not present in table 13.On the contrary, PE0 and PE1 ...

Kraal by Lead
  • 1155 Views
  • 1 replies
  • 0 kudos

ssd1327 oled display interfacing with stm32

Hi have been working on the interfacing of ssd1327 with stm32 microcontroller, i am just trying to print a pixel on the display but I could not display it. my code is as follows WRITECOMMAND(0xae); // WRITECOMMAND(0x15); WRITECOMMAND(0x00); WRITECOMM...

NJP.1 by Associate III
  • 1982 Views
  • 1 replies
  • 0 kudos

Utilizing discover board STM32F407 with FPU

Hello! I am utilizing discover board STM32F407 with FPU , The board is ARM cortex M-4 based. I want to use FPU to quick the process of conducting exponent calculations and Floating point. I have set down all peripheral drivers that are required for a...

by Not applicable
  • 1641 Views
  • 2 replies
  • 0 kudos