cancel
Showing results for 
Search instead for 
Did you mean: 

DMAMUX Synchronization trigger only once

KoRba88
Associate III

I have working sytem with 4 ADC and 4 DMA

Since Im triggering 2 ADC with one Timer (at fixed 25 kHz) and 2 ADC with another timer (at variable 70-240khz) I want to synchronize the DMA data from all ADCs (to the frequency of slower 25kHz timer)

So in one of my slower DMA chanel I have enabled synchronization event with request number 1.

For the faster ADC-DMA channels I have enabled synchronization signal to get it from slower DMA chanell.

Unfortunately in my faster DMA I have recievied data only once and despite the my slow DMA Channel are working.

Im using Cube with LL.

code for dma which syncs all other dma's:

LL_DMAMUX_EnableEventGeneration(DMAMUX1, LL_DMAMUX_CHANNEL_1);

LL_DMAMUX_SetSyncRequestNb(DMAMUX1, LL_DMAMUX_CHANNEL_1, 1);

Code for DMA which shoud be synchronized :

 LL_DMAMUX_EnableSync(DMAMUX1, LL_DMAMUX_CHANNEL_4);

 LL_DMAMUX_SetSyncID(DMAMUX1, LL_DMAMUX_CHANNEL_4, LL_DMAMUX_SYNC_DMAMUX_CH1);

 LL_DMAMUX_SetSyncPolarity(DMAMUX1, LL_DMAMUX_CHANNEL_4, LL_DMAMUX_SYNC_POL_RISING);

 LL_DMAMUX_SetSyncRequestNb(DMAMUX1, LL_DMAMUX_CHANNEL_4, 1);

Should i have to clear some flag (but overrunn is not occuring) or something like that?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Igor Cesko
ST Employee

Hi KoRba88,

Please try to study the DMA MUX synchronization example which is provided within STM32 Cube package for STM32G4: "\STM32Cube_FW_G4_V1.4.0\Projects\NUCLEO-G474RE\Examples\DMA\DMA_MUXSYNC".

Maybe this can help to solve your problem.

Regards

Igor