STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105 unsigned division wrong result

Hello community,Processor : STM32F105 (Cortex M3)Compiler : GCC 6.3.1I would like to execute the following assembly instruction :udiv R3,R2,R3where :R2 = 64 000 000R3 = 1Instead of getting R3 = 64 000 000, I get R3 = 2047I tried to execute strictly t...

JPasc.2 by Associate II
  • 1547 Views
  • 2 replies
  • 0 kudos

DFSDM DMA: Which CPAR register?

Hi - I'm having trouble getting DFSDM input to work with DMA - I'm unable to set the `DMAEN` bit in the DFSDM register.One troubleshooting angle: What register pointer to you pass to the DMA's CPAR? I assume `DFSDM_ FLTxRDATAR` for regular (non-injec...

DOCon.1 by Senior
  • 664 Views
  • 0 replies
  • 0 kudos

STM32F105 Multichannel DMA ADC Read Buffer Offset Error

MCU: STM32F105RCTxFirmware Version: STM32Cube FW_F1 V1.8.0I have DMA setup to read 8 channels of the ADC into a fixed buffer and I'm having an issue where after an extended period of time (usually hours) the ADC channels are read into the wrong buffe...

0693W00000FBEl8QAH.png 0693W00000FBElNQAX.png 0693W00000FBEmGQAX.png 0693W00000FBEmLQAX.png
Jon Enz by Associate III
  • 1638 Views
  • 2 replies
  • 0 kudos

Resolved! DMA using USART3 on STM32H7 part

I am trying to get the USART3 to work with DMA, and so far have been unable to. After the initial cubeIDE project setup, I verified that standard (non DMA) RX and TX were working fine.Moving to DMA, I was getting Direct Mode Error interrupts, and a l...

dawime by Associate II
  • 3381 Views
  • 5 replies
  • 0 kudos

Can QSPI flash store large program memory code?

 Hi,I am using STM32F746G_DISCO board to create different pages for the LCD. I see only one page with 4 tabs project already takes 300KByte flash memory code space. The STM32F746 only has 1MByte flash. So I like to store the LCD graph code related mo...

JChen.24 by Associate III
  • 1640 Views
  • 2 replies
  • 0 kudos

Resolved! usart2 stm32g030k8 does not work correctly

Hello everybody!I can't use USART2 in STM32G030K8 to transfer data.The TC flag of the ISR register is not set after writing data to the TDR register for an infinite time, if I use it to control the transfer of a byte, the program hangs without transf...

Akoli.2 by Associate III
  • 1861 Views
  • 2 replies
  • 0 kudos

The DMA buffer configured with a multichannel ADC setup ( Processor STM32f769II) shows values in different buffer location with respect to the rank configured in the ADC setup. How can this be fixed?

We have connected 7 channels in ADC2 to a STM32F769II processor. The DMA to ADC is enabled and the rank for conversion too is configured. But on testing, the ADC values are being shown in buffer location very different from its rank.This happened in ...

SP.7 by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

STM32L496RET6

please let us know the availability of STM32L496RET6 controller

APara by Associate II
  • 1195 Views
  • 2 replies
  • 0 kudos