STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why does the advanced timer PWM CH1 output affect CH2N?

This is my simulation output waveform.They are CH1, CH1N, CH2, CH2N, CH3, CH3NIt can be seen that CH1, CH2, and CH3 are all normal, but the complementary waveforms will be affected by other channels.How can I configure it?I want to use multi-channel ...

0693W00000FCbMNQA1.png 0693W00000FCbIzQAL.png 0693W00000FCbLUQA1.png 0693W00000FCbM8QAL.png
WFan.1 by Associate
  • 1241 Views
  • 1 replies
  • 0 kudos

STM32F7508-DK UART Tx/Rx Stoppage

With my STM32F7508-DK board, I am interfacing to a BLE board over UART without hardware flow control. Due to pin conflicts, RTS/CTS is not available on that board. My primary issue is when BLE board sends 10K text buffers, STM32F7508-DK UART stops Tx...

EAlta.1 by Associate
  • 955 Views
  • 1 replies
  • 0 kudos

Hardware problem with NSS pin on SPI

I cannot to set NSS pin in push-pull mode. What is may be wrong?I use SPI1 on stm32F7 as a master only mode with SSOE config bit. My system use SPI clock speed 13,5 MHz. GPIOA#4 is used as NSS pin alternative function 5, push-pull output.This configu...

0693W00000FC0s2QAD.bmp
Natsu by Associate II
  • 7271 Views
  • 7 replies
  • 0 kudos

How to use CD4094BE with 74HC595 shift registers

Hi Experts,I have a project like below. I am trying to send the data but the LEDS are not glowing in sending pattern.I am new to STM32F207 Nucleo board. Could anyone please let me know if I am missing anything.STM32f207 ======> CD4094(Q0) ==========>...

Bkris.2 by Associate II
  • 1591 Views
  • 0 replies
  • 0 kudos

Resolved! Current measurement with STM32L562QE-DK

Hello,I want to use the STM32L562QE-DK board to measure the current for my own developed PCBA. There is a connector CN20 that can be used for this purpose as written in the schematic for the board:Output connector to supply and measure external targe...

c_dev05 by Associate III
  • 1315 Views
  • 1 replies
  • 0 kudos

Hi, I'm trying to figure out why my basic timer interrupt on the STM32H7B3x dev board isn't working as expected. It seems to be triggering more often than I expect depending on when I clear the flag within the interrupt.

I am using the STM32H7B3LI-DK dev kit and want to use a simple timer with an interrupt. Using the most basic function, I've added a variable that simply increments within the interrupt. The timer is configured to hit the preloaded value at approx 1ms...

SThom.6 by Associate II
  • 4013 Views
  • 9 replies
  • 0 kudos

How to use function in main.c I want to make function about operate state. using interrupt! Plz check my main code. and check my error. Error[Pe065]: expected a ";

/* USER CODE END Header */   /* Includes ------------------------------------------------------------------*/   #include "main.h"   #include "usart.h"   #include "gpio.h"   #include "stm32h750xx.h"   #include "ESP32.h"   #include "stm32h7xx_hal_uart....

wwgww by Associate II
  • 2250 Views
  • 3 replies
  • 0 kudos