User Activity

Hi,I have a project with an external loader. When programming using ST-LinkV2 (SWD) it works perfectly with CubeIDE or the STM32Programmer CLI.When trying programming the same ELF file using USB DFU connection, I get the following message, and the pr...
Hi,I have found a bug in the designer, how can I report it without exposing my *.tgfx files here in this forum? Roy
Hi,I have a strange TFT flickering issue, and would love to hear your suggestions.The project running on STM32F746 chip, with SDRAM, and LTDC interface. UI is based on TouchGFX & FreeRTOS.Display is 1024X600 RGB (50 pin), based on HX8282 driverhttps:...
Hi,I have a custom board with STM32F746 MCU and XPT2046 touch controller (Clone of TI TSC2046E). They are connected on SPI2 (no other devices on this bus), running at ~210Kbit/s.I couldn't get the touch controller to work correctly, so I've connected...
Hi,I have a project with STM32L010 that runs OK if started from the STM32CubeIDE with the "debug" or "run" buttons, but after power restarts, the code is not running.I have tried to short BOOT0 pin with no success, and I couldn't find a way to progra...
Kudos from