STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F40G UART, unexpected pulse on Rx Line

I am sending some data on UART, When I enable Transmitter TE bit in USART_CR1 register, a pulse is observed on Tx line ( as shown in figure). That's fine but I am observing some 190nsec pulses on Rx lines though I am not sending anything to it! I hav...

0693W00000GWflGQAT.png
IAhma.1 by Associate II
  • 4005 Views
  • 8 replies
  • 0 kudos

Resolved! STM32G030 ADC voltage residual issue

Hi Almighty Internet & STSo huge learning curve using MCU STM32G030J6 with ADCLearned the hard way you cannot use pin 4 for ADC as this is shared by NRST and there is no way to turn off MCU resetting because the bit registers which exist in STM32G031...

MHyst.1 by Associate
  • 1218 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4 problem receiving 0xF8 over UART with HAL

Hello I am trying to send hex values over UART with HAL_Transmitin the cubeIDE I do:HAL_UART_Transmit(&huart2,(0xF << 4) | (0x8), 1,10);However I receive in Hterm0xC5I cannot make sense over it. Sending text with " some text" works fineHAL_UART_Trans...

ABenz.11 by Associate II
  • 2444 Views
  • 4 replies
  • 0 kudos

how to make DAC hold stable output voltage

I am testing OPAMP_PGA example code.Here is the DAC config code: /** DAC channel OUT1 config */ sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC; sConfig.DAC_DMADoubleDataMode = DISABLE; sConfig.DAC_SignedFormat = DISA...

0693W00000GWf1rQAD.jpg
HDaji.1 by Senior
  • 1516 Views
  • 1 replies
  • 0 kudos

iOS app: will not work with STWINKT1B

I wanted to make sure the dev board I received would work before the webinar, but unfortunately I have not been able to reproduce the steps as seen on the YouTube tutorial. It seems like the iOS app is out of date according to attached screenshot.

Resolved! Buffering in STM32F4 uC for UART

I recently got my STM32F407VG uC working with UART4. I can receive a byte and send a byte. Though I have been reading on how to acquire more than one byte at a time. It seems as though people like to use DMA. I am perfectly okay with polling for my e...

JCorl.1 by Senior
  • 10627 Views
  • 6 replies
  • 0 kudos

OC1M set active/inactive on match immediatly changes output

In the capture/compare ISR, I want to program the next CCR1 value and the associated action: to change the output to active or inactive when CNT matches CCR1. For this I need to set TIM1_CCMR1 OC1M to 0001 or 0010. However, as soon as I program OC1M ...

Svan .41 by Associate II
  • 4221 Views
  • 10 replies
  • 0 kudos