STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411 Blackpill : fonction HAL_UART_Receive(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout)

Bonjour,j'ai un système communicant avec des cartes identiques possédant des modules STM32F411 CE8 black pill . une carte est maitre et les autres cartes sont toutes esclaves. je suis en mode "UART_TwoBoards_ComPolling"mon IDE est STM32IDE avec les ...

Joel14 by Associate II
  • 3466 Views
  • 7 replies
  • 0 kudos

STM32L0 Current Drive for GPIO in STOP 0

Hello:Hoping to find out the answer to a question that I cannot find in the data sheet for the part. What is the the drive current used to keep a GPIO pin enabled (SET) while in STOP 0? Page 65 of the data sheet indicates a value of 2.5uA/MHz in ran...

STM32H743 - NUCLEO SPI-DMA not working - always busy

I have attached my sample project with STM32H7https://1drv.ms/u/s!AuUAN7PWAxFS8l9pJ-mzXLp1vpXc?e=oFnJSXIn short, The basic function HAL_SPI_Transmit(&hspi1, aTxBuffer, 2, 1) work fine but it took a long time.For that reason, I tried to use HAL_SPI_Tr...

DPham.2 by Associate II
  • 4325 Views
  • 7 replies
  • 0 kudos

Moving SystemClock_Config Causes Strange Erros

I know this is a vague question, but it's a very strange problem I'm facing. My application (based on STM32G0) is working fine. I used CubeMX to autogenerate all the code, and have been building on top of it. Now I am looking to clean things up a bit...

Konami by Senior II
  • 896 Views
  • 1 replies
  • 0 kudos

Doesn't transmit data via SWO STM32H743

I can not start transfer via SWO to STM32H743.Port PB3 initialized clock feed.Initialized SWO:*(__IO uint32_t*)(0x5C001004) |= 0x00700000; // DBGMCU_CR D3DBGCKEN D1DBGCKEN TRACECLKEN   //UNLOCK FUNNEL *(__IO uint32_t*)(0x5C004FB0) = 0xC5ACC...