User Activity

static void MX_SPI1_Init(void){ /* SPI3 parameter configuration*/ SpiHandle.Instance = SPI1; SpiHandle.Init.Mode = SPI_MODE_MASTER; SpiHandle.Init.Direction = SPI_DIRECTION_2LINES; SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT; SpiHandle.Init.CLK...
/* UART9 init function */void MX_UART9_Init(void){ /* USER CODE BEGIN UART9_Init 0 */ /* USER CODE END UART9_Init 0 */ LL_USART_InitTypeDef UART_InitStruct = {0}; LL_GPIO_InitTypeDef GPIO_InitStruct = {0}; LL_RCC_SetUSARTClockSource(LL_RCC_USART16_CL...
Am using NUCLEO-STM32H723 Nucleo-144 board.Sorry, but I have no experience with the above MCU/TIMx.My goal is to measure external frequency as accurately as possible.I'm interested to know how to Link between two timers.Example : TIM3 ( Master ) TI...