STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F469N - Cannot program option bytes, cannot erase flash.

I've got a custom board with an STM32F469, 32 Mbit of parallel flash, and 64 Mbit of external DRAM. This board had been working fine until an incident where execution or data fetch occurred on the external 32 MBit flash, which had not been programmed...

JVan .3 by Associate II
  • 1236 Views
  • 1 replies
  • 0 kudos

Create a custom cards using STM32L562

Hy,I would like to create a simple Custom cards using STM32L562.My first question is: Do you have a simple schematic with only essentials components ?And my second is:at the first initialisation, the MCU need a BOOTLOAD or particular manipulation (ha...

JCERE.1 by Associate
  • 1961 Views
  • 3 replies
  • 0 kudos

Resolved! how to set RTC alarm for all day in stm32f407vgt?

mcu: " STM32F407VGT Discovery Board - DICS1 "application: RTC ALARMi am trying to set the RTC alarm for every 15 minutes in all the day. in each RTCAlarmcallback function i am setting the RTC alarm again with sTime.Minutes + 15.if sTime.Minute...

Vinay1 by Associate II
  • 3505 Views
  • 6 replies
  • 0 kudos

Resolved! Unexpected Gain in OPAMP_PGA in G431

I am testing Examples/OPAMP/OPAMP_PGA/ in G4 package code, only to find the gain is not consistent as showed below:The OPAMP input values are 0.01,0.03, ..., 0.15, and gain is 16.However, I measured output at ADC side, the gain drops significant as i...

0693W00000GWAeJQAX.jpg
HDaji.1 by Senior
  • 6602 Views
  • 20 replies
  • 0 kudos

Resolved! STM32F7 @ 192MHz: long data copy time?

Hello again,I recently checked the time the STM32F7 (192MHz) needs to copy one 32bit buffer to another one, and I'm a little shocked about how long that takes.(Maybe I expect too much, coming from 8bit µCs with 20MHz, an STM32 still feels like a raci...

LCE by Principal II
  • 3522 Views
  • 10 replies
  • 0 kudos

Resolved! STM32F767's ADC buggy?

I've been sampling some signals using this ADC, embedded in the board NUCLEO-F767ZI but when it reaches the 113th sample, samples are taken wrongly, as I have plotted the memory and the signal shown doesn't correspond the one I am generating. Find my...

SDomí.1 by Associate
  • 1997 Views
  • 4 replies
  • 0 kudos

Issue where flash memory range reads as all zero.

Hello, I’m working on a project using the stm32l562E-DK. The project is based on (mainline) TFM with a secure and nonsecure application, and bootloader. I’ve modified the TFM sector definitions to change the sizes of the sectors. The bootloader and s...

0693W000003RRFTQA4.png 0693W000003RRFJQA4.png
BBekk.1 by Associate II
  • 2665 Views
  • 3 replies
  • 1 kudos

STM32H7 SPI TXP flag not resetting

Hi EveryoneI have a very strange issue in the SPI of my STM32H745.Consider following information0) No Master present on the Bus1) SPI5 is configured in slave.2) No interrupts, no DMA just polling3) Following is the initialization code (FIFO is set to...

0693W00000GVnz9QAD.png
DGupt by Associate III
  • 3256 Views
  • 4 replies
  • 0 kudos