cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, please where can I find any example how to open/write/read a file in the flash for the stm32l4?

CMura.2
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
waclawek.jan
Super User

What FLASH?

JW

Uwe Bonnes
Chief

A "file" is quite a complex concept. What kind of file do you mean?

STM32Cube_FW_L4_V1.16.0\Projects\32L4R9IDISCOVERY\Applications\FatFs\FatFs_uSD_Standalone ??

STM32Cube_FW_L4_V1.16.0\Projects\32L496GDISCOVERY\Examples\FLASH\FLASH_EraseProgram

STM32Cube_FW_L4_V1.16.0\Projects\32L496GDISCOVERY\Examples\FLASH\FLASH_FastProgram

Internal Flash, probably no, its not how people generally approach the problem.

You can create resource trees, or file system type structures, and put them in memory permanently, perhaps wrapping them with file system type access functions to make porting easier.

Perhaps look at MKFSDATA type tools used by LWIP, or similar tools, to create a faux web server

If needing an actual file system, perhap FATFS onto MicroSD cards, or eMMC chips.

Can be done with QSPI NOR Flash, or NAND/NOR Flash generally, but you get to own a lot more of the fine details.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

txt file

Just one, of manageable size, perhaps carve some space in the upper reach of the internal flash sectors, store the data, provide means to erase/write new content.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes a want a small txt file in the internal flash, thanks.

Where can I find any examples? please

I am using the B-L4s5I-IOT01A board