STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FDCAN_Classic_Frame_Networking example

I am using the FDCAN_Classic_Frame_Networking example for the STM32G0 part. Instead of using the 64Mhz clock I have a 16Mhz oscillator connected. The example uses a 1Mb bit rate at 64Mhz. My hardware and ioc file are setup to use the 16Mhz as FDCAN1 ...

BMart.2 by Associate II
  • 810 Views
  • 0 replies
  • 0 kudos

Use one DMA channel with 2 different IPs ?

Hello.The project I am actually working on uses several peripherals such as USART ADC SPI etc. I am trying to use as much DMA as I can, but there is something that I miss in the reference manual and on the internet.Can I use ONE channel with TWO stre...

Aahai.1 by Associate
  • 1745 Views
  • 2 replies
  • 0 kudos

Firmware file for B-L475E-IOT01A_Iot_Node board

Hello,I was testing the B-L475E-IOT01A_Iot_Node board, and the inventek wifi firmware was written incorrectly, and the board crashed.Can I get a firmware file so I can rewrite the entire firmware for this board?

BSalt.1 by Associate III
  • 1459 Views
  • 4 replies
  • 0 kudos

PWM not working?

Hi.This is a really simple question but I don't seem to be able to figure out the problem. I was trying to generate a PWM output (using Timer 2 CH1) on my blue pill board but nothing appears on PA0 after I upload the code.Edit: I am referring to this...

M7890.1 by Associate III
  • 4933 Views
  • 4 replies
  • 0 kudos

Resolved! Count edge with TIM14 channel 1 ?

I use counting on TIM15 and now need change to 14 , but seems here external pulses counting dont work. FYI STM32F030Is any setup for 14 possible?

MM..1 by Chief III
  • 4781 Views
  • 13 replies
  • 0 kudos

Resolved! incorrect nand id stm32h7

Hi everyone First time i read the nand ID with fmc it was all good.It was 0x2c 0xF1 0x80 that the micron told.But some times it couldnt read the id and it was all 0xff.Now when i read the id, i get two different ids.first ox2c 0x1 0x2 0x3 and sometim...