User Activity

Hi there,​My major devices are STM32H747XIH and STM32H743XIH.I prepare to design a board.This board can be replaced with these two devices each other. (Two devices share this board)As I knew about hardware, these two devices are diffenet only in SMPS...
My target device is STM32G474VET6. I checked my empty device that the values are the same with "ST production value" from user manual. (Please see the screenshot) After flash programming on this chip(have done erase and program, no options), I read d...
I would like to implement the flash programming to our JTAG tool.Are there any documents that describe OnCE module and the Nexus read/write (R/W) access block? Such as those described in AN4035. The only thing that AN4035 is inapplicable for SPC58 de...