cancel
Showing results for 
Search instead for 
Did you mean: 

Please help solve the problem STM32H743IIT6

Plee.1
Associate

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Going to need to get a lot more specific with the details

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Plee.1
Associate

Is the description in Chinese ok? This is more accurate, if you need English, we will translate it for you。

 1.使用16M的外部SDRAM作为emwin缓存时,(1366*768*3*2)作为LTDC显示空间,(8192*1024)作为GUI_NUMBYTES分�?给GUI内存。使用当打开�?�缓冲时(RGB565颜色格�?),显示图�?会有定时�?�顿,关闭�?�缓冲正常,但是切�?�图�?时会产生拉窗帘现象。

2.�?�考官方例程移�?LWIP 1.41 LwlP_TCP_Echo_Client,�?使用netconn_connect()函数连接�?务器时,返回结果为ERR_RTE,此时查看网�?��?�侧橙�?�常�?,左侧绿�?�闪�?。使用抓包工具和使用命令行ping机器无法获�?�任何信�?�,如何判断此时的lwip是�?�正常�?始化?

3.LWIP�?�用时,应如何�?置MPU�?护?

4.LWIP使用的内存空间是�?�为AXI RAM?

5.  在调试的时候USB�?�以正常工作,�?�以识别U盘,导出数�?�。断电�?新开机U盘就无法识别,麻烦分�?一下是什么原因。