STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

System Workbench: Doxygen setting blew up compiler

My code was compiling fine, then I turned on the Doxygen setting in preferences. Now i get lots of errors and warnings. My function prototypes say used but never defined. My functions say invalid storage class. I can't find what is broken. I turned o...

Resolved! Help with porting FMC from STM32L4 app to STM32U5

Hi, I'm trying to port my code that uses the FMC to interface a LCD display. The provided configuration works on the STM32L476, but when I port it to the STM32U585 the image is offseted to the right on the display.Main clock (and FMC clock so) are co...

BDELI.2 by Associate II
  • 1417 Views
  • 2 replies
  • 0 kudos

Project for STM32F746 disco with the protocol 61850 Ethernet communication, work with DSP library, working in real-time.

I am trying to make a frequency relay with the STM32F7 disco, for a simulated power electrical systems in real time (OPAL RT); I need to establish a communication between the real time simulator and the STM32F746 dico, through one of the protocols it...

0693W000001sHLhQAM.png
JGARC.1 by Associate
  • 1264 Views
  • 1 replies
  • 0 kudos

Write JPEG data from ov5640 to SD-Card

HiI am doing a project using STM32L496G-Discovery and ov5640 sensor,what I am triying to do is capture data with a resolution of 320x240 and JPEG format and save it to the sd cardhowever when i open the file created I don't see anything.

FTila.1 by Associate II
  • 2890 Views
  • 3 replies
  • 0 kudos