User Activity

Hello All,I need to read tempereture of mcu.But I confused about formula given at referance manual.which is below.Because there no data TS_CAL_2 val   Thanks.Regards.EMRE
Hello All,I am using stm32g030f6 mcu.I have done this project before with stm32f0 mcu and now i am porting it to stm32g0 mcu.flash size of each is 32kB.The project is filling up all the processor's memory.So I used option bytes to keep some values in...
Hello All,I have stm32h745I-disco board.I want USB device as virtual comport.I use cubeIDE and create project with it.I am new on this dual core processors.Thanks to the cubemx it is easy to create a basıc usb code.When I create a usb_fs code with M7...
Hello All,We design a circuit with STM32F030F4.And when I checked the current consumption of the circuit , I saw the curent consumption is changing by the time.It moves like decreasing for some time and increasing suddenly after that decreasing for s...
Hi everyone ,We are using our custom bootloader firmware to update our main firmware.To do that we set a flag at a specific location at RAM and reset the MCU.The flag size is 1 byte.At the bootloader firmware read the data from RAM and if this data m...
Kudos from