STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART mixed flow control

Hello all,I have a device connected to a stm32l496rg on a custom via uart.At system startup, the remote uart may or may not have hardware flow control enabled, so what I want to do is configure the MCU UART for no hardware flow control and put the RT...

DCarr.1 by Senior
  • 2351 Views
  • 2 replies
  • 0 kudos

STM32L4 STOP2Mode

I'm using STM32L476VG and STM32Cube FW_L4 V1.17.1 version HAL Function.I thought STOP2Mode and RESUME work fine.However, when I took the current consumption waveform, it is the same as STOP1Mode.Why is this happening?void Sleep(void) { MX_UART4...

JKim.44 by Associate
  • 930 Views
  • 1 replies
  • 0 kudos

STM32H723ZG Board losing communication

Hi all,Nucleo-144 Stm32h723zg board while debugging suddenly loses communication and shows target not found, unable to read register values. This does not happen always but during debugging this issue is coming up,any solution or any problem with the...

PGM.2 by Associate II
  • 4896 Views
  • 12 replies
  • 0 kudos

STM32F303VC SPI Communication: SPI2 (Slave) SPI1 (Master)

Is it possible to send data from SPI2 to SPI1 ? SPI2 being the slave. In SPI, Master initiates the communication, correct ?This is how i do it:When the Slave SPI2 receives a byte from SPI1, i set a flag, and i check for this flag in main context.If t...

AT.8 by Associate II
  • 2391 Views
  • 4 replies
  • 0 kudos