cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32L471 controller, I just want to ask that what is the maximum value of decoupling capacitor which can be used at JTAG SWDIO pin of controller, so that there would not be any issue during programing of controller using SWD 4MHz setting.

AC1
Associate

I am using STM32L471 controller, I just want to ask that what is the maximum value of decoupling capacitor which can be used at JTAG SWDIO pin of controller, so that there would not be any issue during programing of controller using SWD 4MHz setting.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @AC​, to the community!

Is there a specific reason why you want to connect a decoupling capacitor to SWDIO, as far as I understand from SWDIO to GND?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AC1
Associate

We have defined this JTAG-SWDIO pin as a input in our circuit, during mains as well as in battery mode. To ensure any false detection on input, we need to add a capacitor at this pin, now I just want to ask that what is the maximum value of capacitor that can be used at this pin.

Well, even if connecting a capacitor there is not a good idea - you can roughly estimate that.

Assuming SDIO is driven by the debug interface at 2MHz and its internal resistance is around 20...50 ohms. Then you have a period of 500ns, which corresponds to 250ns pulses (assuming a duty cycle of 1: 1), which results in approx. C = 250ns / (20...50 ohm) = 5...12.5nF. By reducing the SWDIO frequency, the capacitor can certainly also be made larger. Ultimately, there can be no real recommendation for this and must be checked with the setup (connected debugger) provided by you.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.