Receive UART messages in DMA
I am trying to receive messages in DMA mode, on a STM32L432KCU. The pins PA2 and PA3 are configured as DMA pins. The baudrate is 115200 and the global interrupt for USART2 is turned on. In the main function, I have the initialization of the peripherals:
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DMA_Init();, which is followed by the functions that turn on the idle receive mode of the DMA and disable the half transfer interrupt:
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, UART2_rxBuffer, 12);
__HAL_DMA_DISABLE_IT(&hdma_usart2_rx, DMA_IT_HT);Here I have the callback:
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size){
if(huart->Instance == USART2){
memcpy(mainbuff, UART2_rxBuffer, Size);
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, UART2_rxBuffer, 12);
__HAL_DMA_DISABLE_IT(&hdma_usart2_rx, DMA_IT_HT);
}
} It checks if the message is received from the second uart, then copies it into the main buffer, that stores all the data. The receive is enabled again and the half transfer interrupt is disabled. Unfortunately, when I am trying to debug, the breakpoint inside the callback never gets hit. I've also tried to display the message. It didn't work. What could cause this problem?