STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f765xx internal temperature sensor

Hello, I am currently trying to measure the temperature using the internal temperature sensor of STM32F765. The Reference Manual stated to do temp = ((V_sense - V_25) / Avg_Slope) + 25,but the address of calibration data existed in the Datasheet.In t...

STM32U083 wakeup from pin reliability

Hi all,we are designing a product based on a STM32U083. The device is battery powered (not removable) and it can remain in storage for at least 2 years. To reduce battery drain we are putting the mcu in shutdown mode to then wake him up via a button ...

stefanod by Associate
  • 418 Views
  • 1 replies
  • 0 kudos

Extremely Large Binary Size When Using DTCMRAM

Hi, I am working on a project with the STM32H730. In order to make full use of the onboard memory I have the project set up to load some objects into DTCMRAM. This works, however the binary size is huge, like 403 MB, and subsequently is crashing cube...

Screen Shot 2023-12-05 at 9.08.12 AM.png Screenshot 2023-12-05 at 1.12.44 PM.png
EPala.2 by Senior
  • 4724 Views
  • 12 replies
  • 1 kudos

Resolved! STM32L433 NRST pin status

This is a very basic question.I built a custom board using the STM32L433.After applying power (+3.3V), I checked the NRST pin state, but it did not reach the default voltage.Could you please tell me any possible causes?For reference, I have confirmed...

Resolved! MPU causes unaligned access fault

Hi,Master:MCU: STM32H743IIQuestion:I configure the MPU for RAM as follows:mpu_set_protection( 0x24000000, MPU_REGION_SIZE_512KB, MPU_REGION_NUMBER1, MPU_REGIO...

q1.png
Lyu.1 by Senior
  • 492 Views
  • 2 replies
  • 1 kudos

using Dual-Quad-SPI with OCTOSPI in STM32H5xx

Hi,I have been trying to connect PSRAM and NOR FLASH to STM32H563 nucleo board using Dual-Quad-SPI.I was able to successfully read/write to PSRAM and NOR Flash individually in single-Quad-SPI mode with base address 0x90000000. i'm not clear how the a...

shii by Associate II
  • 10227 Views
  • 21 replies
  • 4 kudos

STM32H745 ADC - PA0 Sampling Issue

Hello,On a custom-designed PCB, I am using an STM32H745IIT6 (LQFP176) MCU. I am actively using analog channels, various I/O pins, Ethernet, QSPI, and other peripherals. The code I am using was previously running on an F7 series MCU. It has been fully...

sampleIssueSWV.jpeg samplingIssueExcelGraphic.png

Resolved! STM32H753 STOP Mode inconsistency.

I am using the STM32H753VI chip, it's on a proprietary PCB but the layout is very similar to the nearest NUCLEO board so I am not ready to consider that the issue.I am working on a very low power application, using CubeIDE but minimal HAL, preferring...

KP0 by Associate
  • 561 Views
  • 1 replies
  • 0 kudos

Not able to enable SYSTICK

Hi,I am working with the STM32F103RCT6. I am writing a bare metal code for delay function using SYSTICK timer. The problem I am facing is that I am not able to write to the ARM cortex registers. Below is my code for your reference - This is the stm32...

Screenshot from 2025-09-03 17-52-58.png