User Activity

Please listen to the trouble and cause when debugging with CubeIDE that I was troubled withThe cause is very simple once you understand it, but I couldn't think of it at the time of trouble. Details of the trouble A CubeIDE sample program was execute...
Hi,When the sample program FLASH_EDATA_EraseProgram is executed on the NUCREO-H563ZI board, it appears that 0xAA55 is correctly written to the high-cycle data flash. However, when debugging is terminated and the board is rebooted, the data in the lat...
Hellow! I am trying to use “FLASH_EDATA_EraseProgram” with NUCREO-H563ZI.When I execute the code, it works normally, but when I connect to the debugger again after closing the debugger, part of the EDATA is initialized.When running in standalone mode...
Kudos from