User Activity

Hello,I am using a gate driver IC (1EDN8511BXUSA1) that operates with a 9-10V power supply. The IN- input of the IC is connected to a GPIO pin of the STM32L496, which is internally pulled up to VCC with a 400kΩ resistor (as shown in the picture). At ...
Greetings, I have a problem with LWIP when the D-Cache is enabled. My test program:int main(void){ /* USER CODE BEGIN 1 */  /* USER CODE END 1 *//* USER CODE BEGIN Boot_Mode_Sequence_0 */  int32_t timeout;/* USER CODE END Boot_Mode_Sequence_0 *//* E...
Kudos from
Kudos given to