STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 secure hardware for booting

Hello ,i'm using STM32 board to build secure Boot loader. Currently i'm working on these boards below1)stm32f3342)stm32f4113)stm32f4464)stm32f7465)stm32h723I want to know if this board supports secure boot ? if not could you suggest me which all STM...

Resolved! Minimum HID mouse test code?

I try on nucleo F446 MX_USB_HOST_Init(); /* USER CODE BEGIN 2 */ USBH_ReEnumerate(&hUsbHostFS); /* USER CODE END 2 */   /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ MX_USB_HOST_Process()...

MM..1 by Chief III
  • 1220 Views
  • 3 replies
  • 0 kudos

Socket App 100Mbps STM32F4-Disc

Hello everyoneI have two questions.1-) I'm trying to make a socket app application at 100Mbps with the STM32F407VG DISC card. I want to send and receive data via TCP.2-) I want to measure the read and write time of a port.Can you help with these two ...

Ec1 by Associate II
  • 1525 Views
  • 2 replies
  • 0 kudos

Disable SWD and JTAG by default for STM32F4 MCU

Hi TeamDoes anyone know how to disable SWD and JTAG by default setting, using HAL library?To protect the firmware for reverse engineering, I want to disable SWD.As you know, it is enabled by default after a reset.Also I know that there RDP to protect...

Kenji1 by Senior
  • 1743 Views
  • 2 replies
  • 0 kudos

STM32G4 COMP1 Always triggered

Hi, I'm using comp1 of stm32g474rbt6 and setting 70mV hysteresis.when a DC signal input PB1,the output always shake。But comp4 do not like this.

sliyu.1 by Associate
  • 774 Views
  • 0 replies
  • 0 kudos

UART DMA TX RS485

Hi there!I hope some one can help me. I use one STM32G031F4P6 for one my project, and i use the serial port with one RS485 ic, My problem is that i don't have any problem to receive the data from PC to micro controller the problem is the opposit re...

SGian.1 by Senior
  • 2359 Views
  • 3 replies
  • 0 kudos