STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Center aligned pwm and DMA

How the hell it makes sense to have 2 UEVs per period in center aligned PWM mode and not be able to choose which one generates request for DMA and update of registers. For an interrupt it's possible to choose if underflow or overflow events generate ...

0693W00000QNdahQAD.png
DDona.1 by Associate II
  • 1940 Views
  • 3 replies
  • 1 kudos

How do I wake from Stop mode using UART?

Hello all,After successfully entering Stop mode with my STM32F051, I cannot wake it up. I have referenced this article heavily, but cannot get it to work for me (I see that it is for an F072B): https://github.com/STMicroelectronics/STM32CubeF0/blob/m...

JKing.8 by Associate III
  • 3785 Views
  • 3 replies
  • 0 kudos

STEVAL-IHP005V1(STM32F103x, ST7540) inquiry

Hello, I am a student studying stm32. I bought that module. I want to modify the source code in CUBEIDE. A part of the PLM stack folder is in the form of an object file. Can I get the file in c code?? I don't know the exact email address, so I'm post...

SKim.35 by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

Troubles in Programming USART of NucleoF429

Hi All, I am new in ST microcontrollers. I tried to get messages from the USART module of NucleoF429. i follow the steps in this article: STM32StepByStep:Step3 Introduction to the UART - stm32mcuI used many serial monitor tools such as TeraTerm but I...

Hasan by Associate II
  • 3725 Views
  • 6 replies
  • 0 kudos

STM32L496RGT6 ADC

I'm having serious problems with the ADCI have the voltage I'm reading going through a 47K/100K voltage divider which feeds into an op-amp configured with a gain of 1 and then to ADC1Ch15 on PB0. VSSA is supplied from an external precision voltage re...

DCarr.1 by Senior
  • 2715 Views
  • 5 replies
  • 0 kudos

ADC on STM32L471RGT6 only returns 8 bit values

snippet from main code-> uint32_t a=0; uint32_t ADC_VAL[100]; ADC_VAL[0]=0; HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&ADC_VAL, 1); HAL_Delay(10); a=ADC_VAL[0]; <- set a breakpoint at this point to view the value in 'a' <-      static void MX_ADC1_Init(v...

rwils.1 by Associate III
  • 1983 Views
  • 7 replies
  • 0 kudos

SPI communication with ADS1256 ADC data reading

In my project i have interfaced the STM32 nucleo-f446re dev kit with ADS1256 and when i trying to read the data there is no sclk ticking like transmitting 2 byte of data in logic analyzer there is no data transmission as well as no proper sclk tickin...

Pratyush by Associate II
  • 1735 Views
  • 0 replies
  • 0 kudos