cancel
Showing results for 
Search instead for 
Did you mean: 

Using "HAL_RTCEx_SetWakeUpTimer_IT" with RTC_WAKEUPCLOCK_CK_SPRE_16BITS

MLint.1
Associate II

STM32L5 series Nucleo _L552ZE-Q..

Using Example project "RTC_LowPower_STANDBY_WUT"

The basis of the demo is to count the number of 3 second wakeups from standby, and after 5 wakeups, check the time elapsed =15 secs.

As it is, “out of the box�? works fine.

For my project, I need to do something very similar – except I need much longer periods between wakeups >= 60 seconds.

The example project contains this line:

     if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, wut_value, RTC_WAKEUPCLOCK_RTCCLK_DIV8, wut_value) != HAL_OK)

The Use of clock source RTC_WAKEUPCLOCK_RTCCLK_DIV8 limits the wakeup time to 32 seconds. (Ref Manual 41.3.10 ).

I need much longer times, so I use the ck_spre 1 second clock source instead.

So substituting the above expression above by

if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 2, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 1) != HAL_OK)

I expect a 3 second wake up so the project should still work exactly the same. – but it doesn’t – as soon as the code runs over the “HAL_PWR_EnterSTANDBYMode();�?

it immediately wakes up again !!

Anyone any idea how to get this working ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0