STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1RB availability

Hello, We are interested in developing a product with this MCU but we are not sure when it will be available. Can you help me with some information? We are really early in the dev. cycle and we are not going to "mass produce"(hundreds of units or tho...

Resolved! DUAL MODE DAC OF STM32 F0

I want to create 2 analog output (DAC) on PA4 & PA5 pin. How to make DAC dual mode as instructed in refmanual? When I use template code and add 1 more DAC channel but no success.please help me how to make 2 DACs simultaneously.Thanksstatic void DAC_C...

0693W00000UFH4yQAH.png
Stark by Associate II
  • 1950 Views
  • 1 replies
  • 0 kudos

STM32L4 ADC oversampling setup

I want to use the adc 15bit resolution.I don't understand why right shift and oversampling ratio are at the same time.​1. what is difference12bit + 4bit right shift + oversampling ratio 128xand12bit + oversampling ratio 8x?​2. What are the functions ...

0693W00000SvsRqQAJ.png
hchoi.1 by Associate II
  • 5791 Views
  • 6 replies
  • 1 kudos

I am using STM32H745 Discovery kit. I was running the example provided for UART but unable to see any message in Serial terminal. Checked on CRO but I am unable to see any data transmitted from TX pin (PB10).

I have directly connected the Tx of board to Rx of my computer and Rx of board to Tx of computer through the TTL to USB converter. I also checked the Tx and Rx of the board on DSO but was not able to see any data.

JPere.13 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

STM32H7 why is Dcache faster than DTCMRAM ?

I am benchmarking Stm32h7 processor on floating point operations and using CYCCNT to measure the performance difference .I placed my function in ITCM-RAM. which is just a function that does double math multiplication 10,000 times, the 4 variables use...

xchen.3 by Associate II
  • 6928 Views
  • 12 replies
  • 1 kudos

Resolved! STM32H7 HRTIM Single-shot mode

Hi, I want to use HRTIM to generate active low pulse of width 50ms. The functionality is to generate single 50ms pulse to enable external counter IC. Are there examples to configure HRTIM in single-shot mode.HRTIM kernel freq is 200MHz. Prescaler is...

KGane.1 by Associate III
  • 2578 Views
  • 3 replies
  • 0 kudos

Double complementary death time with STM32-F401RE board

Hi everyone; i followed the tutorial to get two output PWM signal with 10us of death time but i also tried to do a double complementary death time to have 4 signals with rispect death time but it doesn't work. In the main i add two mor command HAL_TI...

SMusc.1 by Senior
  • 2838 Views
  • 5 replies
  • 0 kudos