STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with triple adc Regular simultaneous mode with DMA

Hi, I am trying to set up simple example project with DMA and triple adc working together. What I am getting is that DMA interrupt is only activated once - I verified all the data is trasfered as supposed to. But, next time I start ADC in the for loo...

VRakc.1 by Associate II
  • 3259 Views
  • 4 replies
  • 0 kudos

STM32 encoder mode sample rate

Hello,I'm working on a STM32 project which use the timer in encoder mode.TIM2 of my STM32F103C8 is set in Encoder Mode, I've enabled the TIM2 global interrupt.I'm evaluating the counter at each interrupt.Prescaler is 0, Counter Period is 65535.Main c...

How are MCUs tested for temperature rating?

Hi!I was wondering if anyone has any insight into the temperature rating testing for the STM32 MCUs.Particularly, how can ST establish if a MCU is rated for 85*C or 105*C and how are those differentiated in the manufacturing process?Are MCUs which ar...

MMicl.1 by Associate
  • 1429 Views
  • 3 replies
  • 0 kudos

STM32G474 ADC Communication question

hello.I would like to ask a question about the ADC capabilities of the STM32G474.To use ADC, use the HAL_ADC_Start_DMA function.HAL_ADC_Start_DMA(&hadc1, (uint32_t *)&DATA,1);Here, I know that the third parameter is the number of data to receive.I wa...

KBae.1 by Associate II
  • 780 Views
  • 0 replies
  • 0 kudos

Newcomer questions~Cannot Load Flash Programming Algorithm

As stated in the title~This may be a common problem, but I’m not able to find solution on google.It works fine on my personal laptop, but doesn't work on others PC (Same CMSIS-DAP emulator,same win10,same Keil5.37,same setup).Has anyone encountered d...

ZeroOne by Associate III
  • 1929 Views
  • 2 replies
  • 1 kudos