STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to do a pc waveform display of a four channel adc, it is a serial input pc and the sampling frequency is 1kSPS. What software should I use to develop, the sampling frequency is 2kSPS. I use node-red to find that the chart keeps crashing and can't g

I want to do a pc waveform display of a four channel adc, it is a serial input pc and the sampling frequency is 1kSPS. What software should I use to develop, the sampling frequency is 2kSPS. I use node-red to find that the chart keeps crashing and ca...

Lep by Senior
  • 714 Views
  • 0 replies
  • 0 kudos

Bug STM32F107RCTx SPI REMAPPED NOT WORK

STM32Cube FW_F1 V1.8.4Conditions: SPI1 or SPI3 remapped to PB3-5 pins. Problem: SPI not work.Solution: Enable Debug Serial Wire (PA13 PA14)SWJ function changes SWJ_CFG[2:0] bitsstm32f1xx_hal_msp.c line 81__HAL_AFIO_REMAP_SWJ_NOJTAG();do{ uint32_t tm...

vekli by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos

way to isolate stm32 chipset from NUCLEO board?

Hello, I would like to know the way to measure actual power consumption of stm32 chip on NUCLEO board, so if I disconnect:> LEDs> voltage regulators (supply 3.3vdc directly instead)am I able to get power consumption of stm32 chipset according to its ...

KPrem.2 by Associate
  • 1358 Views
  • 2 replies
  • 0 kudos

Resolved! Can not get SPI_FullDuplex_ComDMA_Master Example in STM32Cube MCU Package for STM32L5 series working on STM32L552E-EV Evaluation board.

I am stuck trying to get the STM32L552E-EV evaluation board running with SPI using the DMA. Neither the mentioned example (STM32CubeL5\Projects\NUCLEO-L552ZE-Q\Examples\SPI\SPI_FullDuplex_ComDMA_Master) nor the code created via the wizard, nor my own...

0693W00000WHjL1QAL.png
HaLed by Associate II
  • 1439 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.