STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stop mode current with NUCLEO-32

Hi,I am using the NUCLEO-32 STM32L011 kit and I want to put the MCU in stop mode to measure Idd. Everything seems to be going well but when I measure the current, this is 2.5µA versus 0.5µA announced in the datasheet when the stop mode is activated w...

Interupt uart not working nucleo g431rb

Hi all i am working in interrupt driven uart uart2 which is connected to the usb port in nucleo -g431rb The interrupt handler is not been called I have shared my code any thoughts kindly share.void USART2_IRQHandler(void) { /* USER CODE BEGIN USAR...

NJP.1 by Associate III
  • 3743 Views
  • 7 replies
  • 0 kudos

Output voltage characteristics of STM32G070CB

Hello folks,I can't figure out the meaning of table 48 p.64 of STM32G070CB datasheet (see attached picture). In particular the FT_c pins. Page 63 it is written that all I/O can source up to +-6mA and +-15mA with relaxed VOL and VOH.Back to table 48, ...

0693W00000WJismQAD.png
Kraal by Lead
  • 2124 Views
  • 4 replies
  • 0 kudos

Resolved! Use RTC wake up in STM32F051 stop mode

Hello.​I am using the stm32f051 discover board.I want to use RTC's WAKE UP function when I wake up in stop mode, is there a way?​The STM32F051 MCU must be used.

THwna.1 by Associate
  • 2962 Views
  • 7 replies
  • 0 kudos

CANBUS nmea 2000 phrase protocol packet on STM32

I have STM32 microcontroller F4 I want to configure the GPS sensor for getting data, I used CANBUS cable and the protocol is nmea 2000, and communicate with HAL_CAN interrupt. my question is, how can I phrase the data from the sensor (on nmea 2000). ...

TBen .1 by Associate
  • 1553 Views
  • 0 replies
  • 0 kudos

I am using the microcontroller in the Nucleo L031K6 model. Our lecturer wants to control LEDs that change according to voltage using ADC and HAL library.

A potentiometer is connected to the breadboard, the middle leg of the potentiometer is connected to the adc pin and the other legs are connected to gnd and 5v.Led (Led Voltage <1V) - Led will be offLed (1V<Led Voltage <2V) - Led will blinkLed (2V < L...

0693W00000WJdF1QAL.png