STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743VG - gap in FLASH bank adresses

Hi,Context:I've hit a roadblock in using the stm32h743VG.According the reference manual, this is the FLASH memory mapping: I'd like to focus your attention on the address gap between Bank1 & Bank2.To alleviate this, I've first done the following:MEMO...

0693W00000WKDp0QAH.png
TGeof.2 by Associate II
  • 2810 Views
  • 5 replies
  • 0 kudos

How to get the FMC ECC working with NAND

I'm using an STM32F765 and a toshiba NAND chip via FMC. I want to use the hardware ECC, but the ECCR register is always empty. My fmc init looks like this: /** Perform the NAND1 memory initialization sequence */ hnand1.Instance = FMC_NAND_DEVICE; /* ...

omisys by Associate II
  • 5339 Views
  • 11 replies
  • 0 kudos

Transfer of the NUCLEO F446Firmware to a new F446 Chip?

I've developed the application on the F446 NUCLEO Board. Now I want to transfer the Firmware of the F446 of the NUCLEO Board to the new installed STM32F446 chip on the PCB. How can this be done or is ther anywere a binary file, that can be uploaded ...

skydiveh by Associate II
  • 1349 Views
  • 2 replies
  • 0 kudos

input capture mode timer interrupt

hello everyonehow can I generate an event when timer operates in input capture mode the counter value goes above the ARR register value? in my special case I load ARR value to 10000 and CNT register goes ablove ARR value and dosent generate an interr...

Msade.1 by Associate
  • 1676 Views
  • 3 replies
  • 0 kudos

Can STM32 chips use any pin?

Coming from AVR this is not possible, I do see some peripherals can use multiple pins. Working with the STM32H7 specifically here. A colleague of mine said he was under the impression ST chips can use any pin ( or a number of pins ) for say one of th...

ulao by Associate III
  • 2453 Views
  • 6 replies
  • 0 kudos

Resolved! Can't flash STM32F411RE from macOS

Hi,i am using macOS to flash an STM32F411RE.It is recognized, the mass storage shows up, but whenever i try to flash it using ArduinoIDE, it exits with code 3: STM32F411RE not found.Does anyone know how to fix this?Thanks in advance.

JNied.2 by Associate
  • 1088 Views
  • 1 replies
  • 0 kudos

Can Anyone guide me in detail how to Measure AC signal 3V, 50Hz using STM32?? I have to find out the RMS value. Since I am new to this can you guide me how to go about ??

I have understood that I have to use Timer to trigger ADC conversion at a configurable sampling frequency. ADC Clock = 24 MHz. I am planning to use DMA also.Can someone help me with calculations and in detail explanation?

STee.1 by Associate
  • 2143 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.