STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using external ram as heap space

Hello,I am working on a project with an STM32H753 Microcontroller and I have an external SDRAM 32 mbyte connected to the MCU via FMC. I want to use the SDRAM as default heap space. This because I want cJSON library use this memory space for dynamic a...

SEfte.1 by Associate II
  • 3145 Views
  • 4 replies
  • 0 kudos

looking for help with a pwm

I have this code that bring a line up for 5us and down for 20. I want to invert it. I thought the first part of the code was a time base loop and the second was also a timer base loop. but one setting effects the other. If I use htim4.Init.Period = 2...

ulao by Associate III
  • 1488 Views
  • 2 replies
  • 0 kudos

Resolved! Erasing a Flash Page of STM32L4R5 doesn’t work

I'm trying to erase a Flash Page of from my firmware Application with STM32L4R5 using the function 'HAL_FLASHEx_Erase()'. The Application Presence Key is stored in this page. It needs to be erased by the Application to activate the Bootloader (this i...

Shadow by Associate II
  • 3098 Views
  • 2 replies
  • 0 kudos

Not Blinking Ld3 anymore

I use STM32GO1291. when I was debugging I got an error (its picture attached in below ) also my LD3 is not blinking anymore. is microcontroller damaged or there is some other things wrong? why it isn't blinking anymore when I plug!

MFara.4 by Associate III
  • 3558 Views
  • 5 replies
  • 0 kudos

Configuring mems microphone and DFSDM on STM32F769I-eval

I'm having some trouble configurating the DFSDM for reading a mems microphone input on STM32F769I-eval. i've followed the instructions on the application note AN5027 and also the tutorial GETTING STARTED WITH ANALOG. In both cases, the input buffer i...

FNegr.1 by Associate
  • 4032 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F429ZI NUCLEO board that supports 6 SPI interfaces

I'm looking for an ARM based MCU that will handle IC configuration on a board in development. Really just need a full breakout for bench testing. I need it to handle at least 6 SPI lines. Comparing available NUCLEO boards to product selector I found ...

RMas by Associate II
  • 3613 Views
  • 5 replies
  • 0 kudos

Resolved! NUCLEO-U575 board, GPDMA destination address update problem

Hello everybody! So what I want to do, is to update the destination address (DAR) register of the DMA after the last transfer. So I write the desired destination address in a variable "dest_address", then I take the address of that variable and write...

Skfir by Senior
  • 1315 Views
  • 1 replies
  • 0 kudos