User Activity

I am now dealing with the work of I2C. As a device, I connect an Eeprom AT24 chip. There are 10K Ohm pull-up resistors. There are no other devices on the bus and nothing else is connected to the boards. Transmission rate 400 kHz.When I connect Eeprom...
I made a firmware download project using a factory bootloader according to AN4286. Everything works fine. I have only one ambiguity - in the description of the bootloader in AN2606 there is a picture on which the SCK signal is pulled-down to the grou...
I`m working with STM32G0 and SPI in slave mode.Is it possible to clear TX FIFO buffer without any master`s clock?In HAL library there is a function called "HAL_SPIEx_FlushRxFIFO", but no method to clear TX FIFO,
I work with STM32G4 and USB PD. I have a question about voltage and current control. How is voltage and current controlled during operation so that the values do not go beyond the limits specified in the profile definition? I found only one place in ...
If it does support EMC, how can I read some ID information from the cable?