STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L431VC - Can VREF+ be sequenced off of VDD/VDDA?

Hello - I am working on a safety critical application using the STM32L431VC that requires the VREF+ voltage rail to be powered off of a different voltage rail than the main VDD and VDDA rail. The VDD and VDDA voltage rails are being generated by a s...

0693W00000WKUiaQAH.png 0693W00000WKUizQAH.png

DAC not responding

I'm using the STM32H745I-DISCO board.I'm trying capture on the ADC and feed straight out on the DAC, triggered by a timer.The timer is working, and the ADC is getting data that looks sensible.I can see data reaching the DAC data register, but the out...

Hardfault Exception Debugging

The Hardfault Exception sometimes occurs during system operation.The register and stack values are as follows after the hardfault exception occurrence.The MSP 0x20003780 points to the stack area storing the register information(LR, PC etc) at the mom...

0693W00000WKbAkQAL.png 0693W00000WKbB4QAL.png 0693W00000WKbIjQAL.png 0693W00000WKbLJQA1.png
Kim.Andy by Associate III
  • 3958 Views
  • 5 replies
  • 0 kudos

hardware fault in stm STM32F733 . need recovery mech.

hi,I am getting hardware fault in stm and i found why it is happening .Now i want to rewrite the below function like clear the Int abd executing next instruction of stack.can i do like that .if possible is there any source code available for that.vo...

kchin.2 by Associate II
  • 2093 Views
  • 3 replies
  • 0 kudos

write internal flash with PVD interrupt

Hi everybody,I use a STM32L476RG. I'm trying to write 4 bytes in the flash memory on a PVD IT.I can write/read in the flash, it works.I've programmed my PVD on level 6 (2.9V) and BOR level is at 1.7V. I've used AN4718 to design a vbat system with a s...

fab04 by Senior
  • 1236 Views
  • 0 replies
  • 0 kudos

Resolved! What is the difference between parts “STM32F429ZGT6�? and "STM32F429ZGT6TR"?Can they be replaced each other pin to pin?Is the software compatible?

What is the difference between parts “STM32F429ZGT6�? and "STM32F429ZGT6TR"? W found from the datasheets,"*** = programmed parts,TR=tape and reel" .We think,“programmed parts�?should not be the same as "tape and reel".So the “TR�? really means?Can th...

ZJian.2 by Associate II
  • 2163 Views
  • 1 replies
  • 1 kudos

FLASH startup code does not branch to RAM

We have an STM32H750 ARM Cortex M7 processor in our product and are compiling C code using STM32CubeIDE. We want to have default code in FLASH that is able to run the default application by itself but which can also load an updated application to AXI...

Resolved! Configuration of OCTOSPI

1.in the manual "AN5050", What's the meaning of "memory type"? Does this mean that OCTO only supports these four types of memory chips? The flash I used is "IS25LP064A", Does the OCTOSPI support this flash?2.How to set the "DEVSIZE"? if the flash si...

0693W00000WK9HTQA1.jpg 0693W00000WK9HsQAL.jpg 0693W00000WK9I2QAL.jpg
rsun.11 by Associate II
  • 5961 Views
  • 9 replies
  • 0 kudos