2025-03-19 7:26 PM
Pls cross TI part number TMP75AIDGKR (Temperature Sensor With I2C and SMBus Interface)
Previously there's a Cross Reference tool in ST website but it's gone. I use it regularly. I hope it can be reinstated.
2025-03-19 10:56 PM
Welcome @eric_copelan, to the community!
The X-Reference search can still be accessed via the homepage. Depending on the browser, either via a drop-down on the left-hand side of the search field or directly in the search results. Just try it out on st.com!
Regards
/Peter
2025-11-17 8:42 AM
The cross-reference option is no gone... it was where we could load it in the search bar and it gives us all available crosses.
2025-11-17 3:05 PM
Welcome @tslater, to the community!
The Xref has not been removed, but is handled differently by different browsers:
Windows Edge
Chrome and, e.g. Brave browser
This is a little more specialised and only allows the above-mentioned alternative function:
I'm sorry that it's so hidden, but maybe this will help you.
Regards
/Peter
2025-12-23 5:38 AM
Hi Peter
I am also facing same issue, I have attached the image for your reference, previously X reference used to come by clicking on magnify glass option but now, I am not able to click on this option.
2026-01-11 11:25 PM
Hi Peter,
I am facing the same issue and cannot find the icon or the name of cross reference in the search bar.
Is this function fully removed from ST homepage?
Thanks.
2026-01-11 11:58 PM
As I mentioned above, the behaviour depends on the browser. Since you haven't provided any information other than the screenshot (e.g. operating system, browser, attempted solutions), it's difficult to formulate an answer.