cancel
Showing results for 
Search instead for 
Did you mean: 

Shared SDRAM via FMC with dual core stm32h745

SNort.1
Associate II

I am seeing the same issue as this question here :

https://community.st.com/s/question/0D53W00000HyV6FSAV/fmc-with-dual-core-stm32h745

I can configure SDRAM access on the STM32H745 for the M7, but when running two cores I cannot get access from the M4 to work at all.

I note that the thread was never resolved.

Is there any guidance documentation on how to configure this, or any sample projects that show both cores accessing SDRAM?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0