Skip to main content
DSchu.9
Associate II
July 18, 2022
Solved

Why is MotorControl Workbench failing to open projects?

  • July 18, 2022
  • 1 reply
  • 879 views

Due to hardware limitations, I must run MotorControl Workbench through the command line. However, running the executable WB_Console.exe fails to open valid projects.

Command issued:

"C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.Y.4\Utilities\PC_Software\STMCWB\WB_Console.exe" -f example.stmcx -generate -Q

This command ideally begins generation without the GUI. However, I immediately get this error:

The project was created with a legacy Workbench release 0.0.0. Please use that version to load the project.
Generation with error.

Given that the example.stmcx is a perfectly valid file (and functions on other hardware), this error is problematic. However, the bigger problem is that the generation will succeed occasionally. I cannot isolate why and have run several tests, including shutting down the system, introducing new (both valid and invalid) files, resetting the software, closing the console.

Regards,

DS

    This topic has been closed for replies.
    Best answer by DSchu.9

    After even more testing, I determined the issue was file paths. While this doesn't address the bugs of occasionally working, it did function enough for my needs.

    My solution: have the .stmcx file path be full (C:\Users\Username\...\example.stmcx)

    1 reply

    DSchu.9
    DSchu.9AuthorBest answer
    Associate II
    July 18, 2022

    After even more testing, I determined the issue was file paths. While this doesn't address the bugs of occasionally working, it did function enough for my needs.

    My solution: have the .stmcx file path be full (C:\Users\Username\...\example.stmcx)