User Activity

I am seeing the same issue as this question here :https://community.st.com/s/question/0D53W00000HyV6FSAV/fmc-with-dual-core-stm32h745I can configure SDRAM access on the STM32H745 for the M7, but when running two cores I cannot get access from the M4 ...
I might be missing a trick here, but it seems that most (if not all) DISCO / EVAL boards expose the same I2C bus externally that is used to communicate with onboard peripherals.This makes perfect sense with DISCO boards as they are small / low cost. ...
I am posting this more as an open question, and perhaps to help someone else...When configuring SAI2 for Audio in CubeMX I had some issues which stemmed from MCLK not appearing to work correctly for the Audio Codec. This would cause the wm8994 to bec...
Firstly come context:I have seen some differences in my sandbox project between what CubeMX auto-generates for my STM32H745I-DISCO and working examples I can download from github. Different GPIO settings which seem significant, for example. The ST gi...