STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743ZIT6 cannot remove readout protection (level 1)

Hello,We activated Readout Protection (level1) on MCU, and cannot revert it.When trying to revert it, it gives "Could not set Option bytes! Please reset the target and retry."error message on ST Link Utility v4.6.0.0.We tried to search the net simila...

CAdat.1 by Associate II
  • 1535 Views
  • 1 replies
  • 0 kudos

Resolved! EXTI15_10 not triggered by user button on NUCLEO-F429ZI

Hello,I'm trying to setup interrupts using the user push button (B1) on the Nucleo-F429ZI board. The push button is connected to the microcontroller through the I/O line PC13.What I did is that I mapped the PC13 to the GPIO_EXTI15 in STM32CubeMX and ...

Fnx_QT by Associate III
  • 12158 Views
  • 22 replies
  • 0 kudos

How to use an AD7768 with STM32H743

I will be working on a project were I need to make a lot of analog measurement very fast. Therefor we are using the AD7768 component from Analog, connected to a NUCLEO-H743ZI development board. I haven't been working with this kind of interface to an...

LKris.1 by Associate II
  • 3771 Views
  • 3 replies
  • 1 kudos

Old date and time on STM32H753 RTC after some days

I'm using STM32H753 on my board and the RTC to get date and time. I'm using the HAL library generated with STMCube. I have set the date and time and the RTC works fine keeping the date and time up to date. The problem is that after more or less 8 day...

STeba.1 by Associate II
  • 4671 Views
  • 9 replies
  • 0 kudos