STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM1 (Input Capture Mode) should DMA one single input Capture value (direct time period measurement, counter reset at every capture) to Memory at every TIM15 counter expiry.

Hello, I want to trigger TIM1 (Input Capture Mode) using TIM15 counter elapse (say every 1 sec). TIM1 should measure input frequency , reset counter every capture, and do one DMA of Input capture value to Memory buffer at every 1 sec (say). I tried P...

BSam by Associate II
  • 5611 Views
  • 9 replies
  • 0 kudos

Resolved! Detailed programming reference for specific boards?

Are there register programming references for specific boards?Its really confusing when there are a whole bunch of "STM32" cpus, that i would think should share common register offsets, but STM32F4 has completely different offsets from STM32L4, for e...

PhilBrown by Associate II
  • 6810 Views
  • 13 replies
  • 0 kudos

Driver for adrv9003

Hey everyone, I tried to write a driver for adrv9003.I tried to do it with stm32h7 controller.So, I tried to use no-os repository from github, and I generated main code with ADRV9001 Transceiver Evaluation Software.I remove the fpga member from initi...

SEliz.1 by Associate
  • 1880 Views
  • 2 replies
  • 0 kudos

We have to purchase electronic components from China Market.(Shen Zhen) China market price is so cheap compare to others. So there is concern about authenticity. Can anyone confirm ?

ST components ( Made in China) from China market(Shen Zhen) are authentic andqulify or not ?Last year we bought STM32F030K6T6 500 pcs at the price of 4.2CNY/pcs.(~0.62USD)And a few thousands of STP75NF75 at 2.4CNY/pcs.(~0.35USD)All components are wor...

AWin4 by Associate
  • 1473 Views
  • 2 replies
  • 0 kudos

STM3240g-EVM Ethernet Ping issue

Hello ST!I am working on Ethernet driver, I used UDP client example application for one of my application development. But the issue is when i connected lan cable to EVM the status LED's which is defined to indicate lan cable is connected is always O...

M_2 by Associate
  • 1846 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 MCU unable to communicate with DPRAM

Hello,I'm working on my customized board with STM32H747XIH6 MCU which is connected to the DPRAM (Part No: 70T653MS12BCGI). The connectivity is as follows.While I'm trying to read and write from the DPRAM after 22 locations the software hangsI have at...

0693W00000Y9RPbQAN.png
Aarra.1 by Senior
  • 5557 Views
  • 7 replies
  • 1 kudos

DMA reset?

I have an A/D circular DMA that collects 192 samples...There can be times when an asynchronous push button event interrupts this while it is collecting. Can someone tell me the quickest solution for resetting the DMA so that after I service the push...

SWenn.1 by Senior III
  • 2395 Views
  • 3 replies
  • 2 kudos

STM32 UART to RS485 Communication bit Shift Problem

Hi AllI have a problem with RS485 Communication. I am using STM32f103rbt6. Only send a struct data (13 bytes). Microcontroller send this data to ADM4855ARZ (RS485 IC). Data sends correctly ( ı checked with logic analyzer). Than this data goes RS485 t...

SCoga.2 by Associate
  • 1123 Views
  • 1 replies
  • 1 kudos