STM32F051 Schematic to connect to ASM330 using SPI
Hi ,Is there any Schematic of ASM330 connections over SPI to STM micro-controller for our Reference design . Please share if there is any reference design of ASM330 connections over SPIThanks
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi ,Is there any Schematic of ASM330 connections over SPI to STM micro-controller for our Reference design . Please share if there is any reference design of ASM330 connections over SPIThanks
Using RTC with LSI Clock, BinaryMode and 24h Format. HAL_RTC_GetTime/Date returns unpredictable values after stop mode crossing midday or midnight:hours value above 24h. see a)"pm" (Timeformat "64") in 24h Mode, which is sometimes wrong additionally,...
Hello,I am using the comparators (COMP2) on STM32G4 and want to add some blanking windows to let the COMP2 input get rid of the system switching noise.The technical manual gives a very brief example as shown in Fig.1. But I need something more compl...
We will use chips with lower data witdh than 32 bits, by this we put multiple chip form the data bus.Could you help me?
Hello every I have One doubt in stm32 I am send the frame formate in Docklight but I cant able to check my frame using without interrupt .anyone give the solution/* USER CODE BEGIN Header */ /** *****************************************************...
Hi everyone,I am trying to send data from one STM32G0B1 MCU to another STM32G0B1 MCU. When i use standard ID it works perfectly but if i use Extended ID then the receiver interrupt doesn't fire. I also checked it with logic analyzer. Transmitter send...
RM0440 Rev 7 (STM32G4), 39.5.12 NSS pulse mode.It is written on the page 1753: “This mode is activated by the NSSP bit in the SPIx_CR2 register and it takes effect only if the SPI interface is configured as Motorola SPI master (FRF=0) with capture on...
Can STM32L151C8T6/STM32L151CBT6 download ISP with one click?Can you provide a reference circuit diagram?
Hello All,I am adding parts of my code. Storing to flash is working if I DMA TIM1 CCR1 to memory and then copy from memory buffer to Flash.I assumed that writing to QSPI_DR will trigger transfer to Flash.Is it feasible to DMA to QSPI?////////////////...