User Activity

I was working with the test code of QSPI. I generated the code using the latest STM CUBMX ver 1.10.1. But after generation also it didn’t worked. Then I compared the code with the sample test code. There I found the below mentioned code patch in the ...
I am using STM32H757I-Eval Board for our study, I created the project for STM32H757 SDRAM interface. While configuring the SDRAM through FMC. I configured SDRAM1 with Bank 2. After that found that the pin configuration generated by the code genera...
Hi,I am using STM32H757 Evaluation board . I created dual core project using by referring the below linkhttps://www.youtube.com/watch?v=jI1k6p-fduEI was able to create the project and compile the same as per the instruction mentioned in the above lin...
we started evaluating the controller architecture with respect to our application requirement. We are referring application note AN5557, Reference manual for the suggested MCU.While referring the documents, we understand that there are 3 Domain in th...
Kudos from