STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UART2 doesn't sent data from TX

Posted on July 20, 2017 at 06:03I made a program and it works well without UART2. I just made a simple program but nothing happend on the TX pin of the UART2.while (1) { /* USER CODE END WHILE *//* USER CODE BEGIN 3 */displayBuffer[0]++; updateLcd()...

Changing filter and channel properties during the run

Hi,I'm using DFSDM on NUCLEO-L476RG, the DFSDM configured as follows:static void MX_DFSDM1_Init(void) {   /* USER CODE BEGIN DFSDM1_Init 0 */   /* USER CODE END DFSDM1_Init 0 */   /* USER CODE BEGIN DFSDM1_Init 1 */   /* USER CODE END DFSDM1_...

lFurm.1 by Associate II
  • 3300 Views
  • 1 replies
  • 0 kudos

cannot debug, throwing the error

I accidently clicked on device configuration tool code generation icon i believe and i am now unable to run the code. I am getting these bunch of errors. How do i solve this problem?

0693W00000aIA5pQAG.png
RShre.2 by Associate III
  • 716 Views
  • 2 replies
  • 0 kudos

FMC Nor Flash XIP with STM32H7

Hi I have a custom STM32H743 board with FMC nor flash M29W128GH70ZS6, and I want to run code on this FMC nor flash.I noticed there is anexample project in STM32Cube_FW_H7_V1.11.0\Projects\STM32H743I-EVAL\Applications\ExtMem_CodeExecution\ExtMem_Appli...

Hello, the STM32F030C8T6 chip I recently bought has repeatedly reset after the burning program, and can only be burned once. After the first successful burning, after the reset by external keys, the chip reset pin will continue to output triangle waves, r

您好,我最近买的STM32F030C8T6芯片在刻录程�?�?��??�?�?�?,�?�能烧录一次。第一次烧录�?功�?�,通过外键�?�?�?�,芯片�?�?引脚会继续输出三角波,导致芯片无法正常�?�动,无法�?次烧录。您�?�能在移除外部晶体振�?�器�?��?新连接STM32 ST-LINK实用程�?刻录工具进行下载和刻录。连续七个芯片都是如此。你之�?买的薯片烧完�?�就正常了。�?然间,这个问题无法解决。检查电路�?�接线�?�?�?电路和晶体振�?�器电路是�?��?�正常。MC...

ayang.11 by Associate
  • 1589 Views
  • 1 replies
  • 0 kudos