STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Transmitting and Receiving Data Not Matching

Hello,I control an ADC with SPI interface of the STM32F44 microcontroller. The ADC datasheet is in the link, https://intantech.com/files/Intan_RHD2000_series_datasheet.pdf . I set up global variables as read, write, and calibrate masks. The I call t...

_legacyfs_online_stmicro_images_0693W00000biGAhQAM.png
AE104 by Senior
  • 4289 Views
  • 9 replies
  • 0 kudos

QSPI External flash loader

"I want to make a QSPI flash loader and I'm watching ST's video series (it's a bit old). I'm using an STM32F446RE. Are the function prototypes shown in the video sufficient for the flash loader to work? Do you have any advice you can give me?"

High sampling rate with ADC and no DMA

Hello All,I have some questions regarding the ADC of the STM32G071RBT6. Technically we can reach a conversion time of 400 ns if we use the internal ADC clock (35 MHz) and a sampling time of 1.5 cyc. OK, that's pretty good idealy.I am running my micro...

izamfx by Associate
  • 1846 Views
  • 2 replies
  • 0 kudos

Resolved! Data coherency with DMA and I2S audio on STM32H7

Moving from a audio effect prototype based on the STM32F407 to the STM32H757. Did a lot of stuff on the F4 with audio but on the H7 I'm getting stuck and can't get a simple audio loopback with DMA. I'm using Cirrus Logic's CS5343 and CS4344 as extern...

Alefal by Associate III
  • 13796 Views
  • 18 replies
  • 1 kudos