2022-11-24 6:31 AM
I use the STM32H745 under the CubeIDE. I thought, when I configure my ADC to trigger the interrupt from a timer, the HAL_ADC_ConvCpltCallback() function will becalled automatically. The related ISR is called and I can read out the value. But the Callback-Function is not reached anymore.
As you see, I have the HAL_ADC_ErrorCallback() in my code, which a called everytime. But the Errorcode is zero. My assumption would be, with a errorcode Zero, the errorhandler will not be called. Is this behaviour wanted?
Third point is, if I set a breakpoint before the HAL_ADC_ErrorCallback(), e.g. line 7 in the TriggerCallback(), the debugger is jumping in the HAL_ADC_ErrorCallback(). What's happen here? The HAL_ADC_ConvHalfCpltCallback() is from my experiments to work with the DMA-Channels.
--- section from my sources ---
void TriggerCallback(TIM_HandleTypeDef *htim)
{
adcConvComplete = 0;
// printf("Trigger Callback\n");
}
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc) {
adcConvComplete = 1;
printf("\033[7;1H ADC %d : ", adc_buffer[0]);
printf("%d :", adc_buffer[1]);
}
void HAL_ADC_ErrorCallback(ADC_HandleTypeDef *hadc)
{
static __IO int x=0, error;
error = 1;
error = (uint16_t)HAL_ADC_GetError(&hadc3);
// if ( 0 != error)
MYDEBUG("DMA Callback: %d %d\n", error, x++);
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
adcConvComplete = 1;
uint32_t result;
result = HAL_ADC_GetValue(&hadc3);
printf("\033[8;1H ADC Cplt %d : ", (uint16_t) result);
}---IRQ-Handler from *it.c---
void ADC3_IRQHandler(void)
{
/* USER CODE BEGIN ADC3_IRQn 0 */
NVIC_ClearPendingIRQ(ADC_IRQn);
HAL_ADC_Stop_IT(&hadc3);
/* USER CODE END ADC3_IRQn 0 */
HAL_ADC_IRQHandler(&hadc3);
/* USER CODE BEGIN ADC3_IRQn 1 */
// ADC3Val = HAL_ADC_GetValue(&hadc3);
// printf("\033[9;1H ADC Cplt Int %d", (uint16_t) ADC3Val);
/* USER CODE END ADC3_IRQn 1 */
}
2022-11-24 8:19 AM
You dont show start code and completely dont understand your idea. Complete IRQ is used for big buffers and multi conversions. Read examples from firmware repository folders
.
2022-11-24 8:25 AM
Hi,
I start my ADC from a timer (not part from the sequence above). My aim in my project is, to read out a sequence of 4 channels from ADC3 via DMA. This is not working right now and I was going back to read out just one channel with interrrupt. And while doing this, I saw, the handler is reached, but the callback function isn't. The strange behaviour with the breakpoints s a side effect.
Jan
2022-11-24 8:58 AM
For start use bigger sample times, If your plan is sample four channels one sample , why not with pool method.
And HAL callbacks is based on ok IT file, you kill it with
---IRQ-Handler from *it.c---
void ADC3_IRQHandler(void)
{
/* USER CODE BEGIN ADC3_IRQn 0 */
NVIC_ClearPendingIRQ(ADC_IRQn);
HAL_ADC_Stop_IT(&hadc3);
/* USER CODE END ADC3_IRQn 0 */
HAL_ADC_IRQHandler(&hadc3);
/* USER CODE BEGIN ADC3_IRQn 1 */
// ADC3Val = HAL_ADC_GetValue(&hadc3);
// printf("\033[9;1H ADC Cplt Int %d", (uint16_t) ADC3Val);
/* USER CODE END ADC3_IRQn 1 */
}
2022-11-25 7:55 AM
To let the IRQHandler untouched was new for me. This solves my problem with the callback function. Thanks.