STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Controlling the ad5675r using the stm32's HAL library

Hello!I am a beginner and I am trying to implement a simple I2C communication with the DAC AD5675R using the STM32h723zg Nucleo board, I would like to start by having the first channel of the DAC output a voltage (say 2V). I have connected the +VOUT ...

DXu.5 by Associate
  • 1111 Views
  • 0 replies
  • 0 kudos

Failing to use SWAP Output 1 and Output 2 function.

Hi, I am trying to use SWAP Output 1 and Output 2 function for HRTIM running with the deadtime function enabled. The description for SWAP function in ref manual says that "the HRTIM_SETA1R and HRTIM_RSTA1R are coding for the output A2, and the HRTIM_...

MYAQO.1 by Associate II
  • 1649 Views
  • 1 replies
  • 0 kudos

The STM32L431 RTC clock is slowing down

We tested the RTC clock and found a phenomenon that the system kept VDD3.3V in standby state and then disconnected VDD3.3V in standby state, but the RTC clock did not run slowly. If the system controlled automatically and disconnected VDD3.3V in slee...

_legacyfs_online_stmicro_images_0693W00000bkPU6QAM.png _legacyfs_online_stmicro_images_0693W00000bkPULQA2.png
Kevin.YIN by Associate II
  • 3111 Views
  • 4 replies
  • 0 kudos

How to interface an external ADC for highest speed?

Hello, I am planning to use the STM32H7A3ZI for a personal project and want to achieve the highest speed possible with an external ADC while storing at least 16 million samples in an external memory. In the tenths or hundreds of MSPS range, ADCs tend...

R.uy by Associate II
  • 5632 Views
  • 5 replies
  • 0 kudos