User Activity

Hello all,I am testing low power mode 2 using ThreadX but having a bit of a problem when waking up. I have generated a simple test, there is one task running blinking a led every second for 10 secs and then sending the MCU to low power mode 2, until ...
I am facing a problem when trying to wake up from Stop2Mode. I am able to come out of stop2mode from an external interrupt with no problem but when using wakeuptimer interrupt the unit doesn't wake up.I have tried that setting the wakeup timer interr...
Posted on July 09, 2018 at 14:13Hello all,I am using the DTM for bluenrg-1 I can program the unit and it will work fine but for some reason when the unit is left powered down for a couple of hours and then powered up again some times stops working.D...
Posted on March 20, 2018 at 15:26Hello,Having connected two bluenrg-1 devices, if I send a new update value from the slave to the master, is there any way of receiving a confirmation from the master to the slave when I send that new value to know if...
Posted on March 13, 2018 at 09:39Hello all,I am facing a problem to update the values when changed. I have an slave bluenrg-1 stand alone which has defined 1 service and 5 characteristics and a master running in coprocessor which has defined 1 servi...