STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h745 phy

hi, i want to implement ethernet communication between two stm32 boards without using phy, but only gpio's connected by jumpers. how can i disable the phy?

Ilay2002 by Associate
  • 1495 Views
  • 3 replies
  • 0 kudos

Impedance control for high speed SPI

Hello,We are a company making medical air transport containers. We use ST micro-controllers (STM32L562ZET6Q) to track, monitor and control our containers around the world.We are having issues with signal integrity between our micro-controller and our...

New batch 3MHz.jpg New batch 13MHz.jpg Old batch 13MHz.jpg
sagan by Associate
  • 4510 Views
  • 4 replies
  • 1 kudos

Resolved! STM32U599NJH6Q

Is this device in the witness protection program? Anglia cannot export the device outside the UK. Contacts for ST office in Canada are not listed. Good job. DK / Mouser list prices at 2-3x those on Anglia with 0 stock and ETA of the end of this year....

Mon2 by Senior III
  • 1471 Views
  • 1 replies
  • 1 kudos

STM32L052T6Yx usb(virtual port com) to pc

I want use this mcu STM32L052T6Yx  to communicate via usb (virtual port com ) whit pc (whith linux system operativ).THE power supply of mcu is 3.3v, can I problems if i directly connect PA11 PA12 PIN  to the pc usb (common ground)? , moreover  on pin...

Combined UAC + HID functionality with STM32L452RE

Hello,I am new to the forums here! Can STM32L452RE support a combination class of HID and USB Audio Class over USB 2.0 Fullspeed?Ideally, I'd like to read and send microphone data (or any sensor data for that matter) connected to STM32L452RE over USB...

bntess by Associate
  • 1746 Views
  • 1 replies
  • 0 kudos

SPI data size reducuction to 1-bit

I have a rather strange request, but I am communicating to a Digital Potentiometer (AD5227) over SPI.  The chip has 64 available positions, but can only increment or decremement its position by 1 for each clock cycle.  To increment by 1, a 1 is place...

JSext.1 by Associate II
  • 5413 Views
  • 12 replies
  • 1 kudos

STM32F 407 &&& 2 USB MASS STORAGE DEVICE

Good evening guys, I have an educational project for the USB protocol on the stm23f407 discovery board I made the project on two sensors and each sensor is written to a flash drive on a separate usb_otg_host port because the stm32f407 discovery board...

Resolved! STM32H723 ADC read stuck (using LL libraries)

Hello,In my project I just sometimes need to read ADC values. I figure I could simply connect two of my signals to ADC1 and ADC2 respectively.What it strange that it does sometimes working, but sometimes it is stuck at constant value ( maybe first re...

Linas L by Senior II
  • 2878 Views
  • 4 replies
  • 1 kudos