STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About I3C ENTDAA ,How to do End DAA procedure waveform?

hiI do the ENTDAA protocol use this codeif (HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, 0) != HAL_OK){/* Error_Handler() function is called when error occurs. */Error_Handler();} In below picture , I get the ENTDAA Protocol, but After protocol there should...

CLHUANG_1-1690457730965.png CLHUANG_0-1690457717715.png CLHUANG_2-1690457746444.png
CLHUANG by Associate III
  • 7555 Views
  • 12 replies
  • 1 kudos

Re: STM32 CAN transmit bug?

Same problem here.. can you please look at this issue STM as it cant be the boards .. hence every single thread on this problems goes cold a working Interupt enabled RX TX example with the latest STMCube/HAL would be nice For STM32F4xx

NCD by Associate II
  • 1148 Views
  • 1 replies
  • 0 kudos

Resolved! why I3C NACK (use the NUCLEO‑H503Rb and X-NUCLEO-IKS01A3 )

I used the NUCLEO‑H503Rb and X-NUCLEO-IKS01A3 boards to do the I3C protocol sample to get the sensor data on X-NUCLEO-IKS01A3 boards.I use the I3C sample program in STM32CubeIDE 1.13.0When I press the USER button on the board, and I get the following...

CLHUANG_2-1690199706649.png CLHUANG_0-1690200085708.png CLHUANG_1-1690199627806.png
CLHUANG by Associate III
  • 2992 Views
  • 5 replies
  • 0 kudos

STM32 as I2C slave: Data recieved LED not working

I'm trying to setup an STM32F401RBT as an I2C slave with an Arduino Uno as the master. The Arduino code looks as follows: I'm simply trying to transmit "3". The STM32 side looks like this: I use these three callback functions to manage the data. I am...

SwissGnome_0-1690267011304.png SwissGnome_1-1690267097195.png

Resolved! DMA to read multiple ADC Channels

I am trying to read multiple ADCs using DMA on a Nucleo H743ZI2. I currently have code that works, but it only works when my data buffer has a size of 32. This is fine when I was using two channels, but any more than that, it offsets the data, and I ...

APBashara by Associate II
  • 3259 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F103C8T6 SPI not working on custom board

Hi I am running WS2812 addressable LED on stm32 bluepill without any problem.I have used SPI to generate data for WS2812 led strip data pin is connected to PA7 (MOSI) pin on bluepill. till now everything is working perfectly fine. So I design a custo...

sandeep3 by Associate II
  • 10703 Views
  • 3 replies
  • 1 kudos

stm32co debugger/programmer

Hi,I am using a prototype with stm32c011f6p6 MCU to program that Can i use STM32F40 discovery kit.I used but I couldn't able debug.I need to is it possible or I need to buy a separate programmer.any issues with hardware i couldn't able to find out.ca...

SRAM.11 by Associate III
  • 1235 Views
  • 1 replies
  • 2 kudos

RTC Clock on GPIO_Input PC13

I'm currantly working on STM32G4 series and I had a problem. I initiate PC13 pin as GPIO_INPUT to read state from button. But It is possible to config this pin(PC13) such as RTC_OUT1. I config my RTC clock on Activate Clock Source to write and read a...

ST_library.png
Mongolov by Associate II
  • 4930 Views
  • 8 replies
  • 0 kudos