STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F769I-DISCO

Hello.I am developing a product with STM32F769I-DISCO development kit.Unfortunately, by my mistake, I think I connected 24VDC to the power terminal, so I couldn't use the power IC that looked like a regulator marked U4.Can you check the exact name of...

R3D3 by Associate II
  • 3997 Views
  • 4 replies
  • 4 kudos

Power Wake UP

Hi,Im using stm32h7 mcu for my project.Which is an iot product.I need to use low power mode on it  i need to wake the mcu using an gpio external interrupt or either by an uart .Device is switch to some mode with a constant current consumption which i...

Resolved! STM32F4 - Fade and Loop Debugging Help

Greetings,I have been working with the STM32F407ZG and a KnobG Click from MikroElectronica. I read the datasheet for the PCA9956B and have managed to address the device successfully at the address of 0x70. Now then according to the usage I have seen ...

Resolved! STM32 Ethernet RMII set up issues

Hey all, I've been working on this issue for about a week and am still not gaining any traction. I am trying to set up the RMII for the STM32H723ZG eval board (I cannot use the MII as we are using the pins for other peripherals).The LwIP TCP echo wor...

cjbruff_1-1689880164929.png cjbruff_2-1689880180087.png cjbruff_3-1689880193359.png cjbruff_4-1689880211886.png
cjbruff by Associate II
  • 5532 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G03 DMA initialization causing uwanted effects on Systick

Hi everyone,Im havinga annoying problem, im trying to inialize the DMA with the ADC , on my custom board. when a initlize it, it works fine, i get the 3 values of the trhee adc channel stored on a buffer. But the Systick timer goes crazy. i get way m...

yIzumi by Associate II
  • 3202 Views
  • 5 replies
  • 3 kudos

stm32c011

please let me know my coding is correct ,whether usage of my exti is correct  while (1) { HAL_Delay(300); // MAINS INPUT Adc_Mains(); HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1,1000); Main...

SRAM.11 by Associate III
  • 1083 Views
  • 0 replies
  • 0 kudos