STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745XIT6 MT25QL256A External Loader not working

Hi every one ..I designed custom board for stm32h745xit6 .My TouchGFX working fine with internal flash .The core board has mt25ql256a and connected as under PB2 CLKPG6 NCSPF8 D0PF9 D1PF7 D2PF6 D3I generated STLDR as explained in ST videos tutorial.my...

_legacyfs_online_stmicro_images_0693W00000dDVHjQAO.png _legacyfs_online_stmicro_images_0693W00000dDVHoQAO.png _legacyfs_online_stmicro_images_0693W00000dDaFdQAK.png
INaee.1 by Senior
  • 4527 Views
  • 5 replies
  • 1 kudos

USB HID Host MX_USB_HOST_Process Call

I've setup my STM32L475 non-RTOS as a USB HID Host to interface with a barcode scanner.  All works well if I call sdf MX_USB_HOST_Process in my main application loop with no delays.  However, if MX_USB_HOST_Process is not called fast enough, characte...

Stanford by Associate II
  • 1892 Views
  • 1 replies
  • 0 kudos

Resolved! Writing data on internal flash of STM32f76

Hello, I want to take data from ADC input and store them on the internal flash memory of my STM32f769i-discovery board. Can you help me about the use of flash memory? Thank you.

elif79 by Associate
  • 1883 Views
  • 2 replies
  • 2 kudos

Resolved! STM32G0B0 USART1 data incorrect

- STM32G0B0 USART1 receiving RS485 data via interrupt driven data collection.   Our micro is attached to a RS485 interface(38400, 8,N,1) receiving BACnet data. The data taken on the 485 bus is different from what we receive in the USART buffers. We h...

Capture.JPG RigolDS0.jpg Capture.JPG

Resolved! How PLL affects timer Pre-sclaer.

Below i have attached a code which enables the PLL freq of 72MHz using HSI of 16MHz. The issue is if I give a Timer pre-scaler of 36000-1 (I am using timer2, which in case of STM32F401RE is on APB1 bus so using a pre-scaler of 2 for APB1 which makes ...

DJ1 by Associate III
  • 8017 Views
  • 12 replies
  • 2 kudos

Resolved! UCPD activation crashes STM32U5 MCUs - hardware bug?

Using Nucleo-U575ZI-Q (rev X) board I try to do a PoC - a very simple UCPD source app providing default USB 5V and 0.5A max. With undocumented onboard SB8-10 shorten this probably can be accomplished. I know this board does not provide output current...

TDJ by Lead
  • 10720 Views
  • 20 replies
  • 4 kudos